THVD2450: Measurement - VIT+ / VIT- for RX receiver

Part Number: THVD2450

Hello,

I am trying to build a testbench using THVD2450, and I need to measure accurately the thresholds VIT+/VIT- for the receiver. I could not find the procedure explaining how this threshold has been determined in the component datasheet.

Could you explain and/or send a schematic explaining the setup?

Thanks in advance for your support.

Best regards,
Timothee

  • Hi Timothee,

    Good question here. I don't think we have a document covering this, but it would likely be worthwhile to create on our end.

    So to start, THVD2450 does have these thresholds already listed in the datasheet (labeled as VTH+ and VTH-). 

    But if you want to validate this, you'll need to mimic Figure 7-3 in the datasheet (namely ~54 to 60 Ohm bus load and ~50pF). Then what I recommend to simplify the measurement is to keep one of the two differential pins at a constant voltage (i.e. the A pin). This makes the differential voltage calculation (A-B) much easier. With the A pin fixed, either raise or lower the B pin voltage with a power supply in a positive going or negative going direction until you see the R pin switch states. Then the VTH is the voltage of A-B when the R pin toggles. Note that you will want a decently accurate power supply and an voltmeter/oscilloscope to validate the supply's output voltage. 

    Let me know if that makes sense or if you have other questions.

    -Ethan

  • Hello Ethan,

    Thanks for the quick and detailed answer!

    I understand what you are suggesting, though a few questions remain for me. From my understanding of the IC, the circuit has a threshold for the fail safe, that falls between -40 mV and +40 mV, and a delay of 10 µs to enter the fail-safe condition. If I increase the signal on pin B slowly by let's say 10 mV steps, I will probably fall in a case where -40 mV < A - B < 40 mV, and this ramp-up step period will be longer than 10 µs. The circuit will then consider it to be a fail-safe condition, even though it is not, and I will miss the operating threshold voltage measurement.

    Does this make sense?

    Timothee

  • Hello Ethan,

    Thanks for the quick and detailed answer!

    I understand what you are suggesting, though a few questions remain for me. From my understanding of the IC, the circuit has a threshold for the fail safe, that falls between -40 mV and +40 mV, and a delay of 10 µs to enter the fail-safe condition. If I increase the signal on pin B slowly by let's say 10 mV steps, I will probably fall in a case where -40 mV < A - B < 40 mV, and this ramp-up step period will be longer than 10 µs. The circuit will then consider it to be a fail-safe condition, even though it is not, and I will miss the operating threshold voltage measurement.

    Does this make sense?

    Timothee

  • Hi Timothee,

    Yep, you'll want to stay outside the -40 to 40mV range so the failsafe function doesn't trigger and set the R pin low. 

    What you can do is have a larger step up voltage when you are close to the +/-40mV range. So for the positive going VTH+, you can start with a negative -VID (VID<-1V), then jump to around ~40 to 60mV. After ~60mV, you can continue with your 10mV steps until around 125mV when the typical threshold trigger point is.

    Best,

    Ethan