Part Number: TMUX4053
Hi Teams,
S1 \ S2 input 5V square wave, SEL1 \ SEL2 are 5V high level, VDD is 24V
Recently, the customer has discovered three devices with abnormal output on these two pins; SEL1 \ SEL2 maintains a high level after power on, with square waves input from S1B \ S2B. One of the faulty devices D1 \ D2 outputs a square wave normally, while the faulty one continues to be at a high level, with the high level value equal to VDD level. Some of these three devices have abnormal D1 output and others have abnormal D2 output. Please help investigate the possible causes of this phenomenon.
Thank you!