DP83869HM: DP83869 MDIO Returning Constant Value

Part Number: DP83869HM

Hello,

We have a custom board with two DP83869HMRGZT. Their MDIO/MDC interfaces are tied together to an upstream processor that is capable of communicating to both of the PHYs. We have a few of these boards built and have noticed that, on several boards, the MDIO returns from one of the PHYs will be a constant 0x7949 (regardless of what register is being accessed). We can still communicate with the other-"good" PHY over this same MDIO interface with no issues/concerns.

I'm trying to deduce what state the PHY must be in to perform this way and how to rectify this. Any ideas?

Attempts at resetting the PHY using an external reset does not change the behavior. Attempts at communicating with the PHY over the MDIO interface to perform a reset/shutdown do not change the behavior. We have validated that the voltage rails powering the device adhere to the documented recommendations/requirements. Attempts at communicating with a non-viable address over the MDIO interface return 0xFFFFs as expected.

image.png