Part Number: TCA9617A
Hello,
I am using the TCA9617ADGKR to drive an I2C signal from an STM32F427 processor to an I2C IO expander (the IO expander is off the board and attached via a 3 foot cable). I'm attaching a snippet from the schematic showing how we set up the TCA9617A part. Also, as a note, in the datasheet I see you show 240 and 820 ohm pullups which do not make any sense to me because those would be strong pull-ups. As you see on my schematic, we are using 10K pull-ups. In addition to the schematic snippet, I am posting 2 scope snapshots. They are both the same, but one is an overlayed version of the clk and data signals to better show the voltage offset this part introduces and the distortion of the signals. I've annotated the scope snapshots, but I'll say just a few words here. The input to the TCA9617A looks nice, the output is very distorted and has a voltage offset which is causing the downstream IO expander to not understand the message. Why is the signal so distorted? Also, please note there are NO series resistors between the micro and the TCA9617A.