Part Number: DP83TD535EVM
We are evaluating a DP83TD535EVM (S/N 2766543) and struggling to get it to behave as per documentation.
Power, gnd etc. is all within correct spec and operation with a valid link partner.
The EVM grounding is somewhat odd but we joined GND to S_GND to have a valid gnd connection to the PMOD connector interfacing to our control FPGA.
Regardless of whether the media side is floating or tied to a T1S link partner, after POR or a reset pulse issued on TX, the ED & RX pins remain high and never transition or pulse low.
They are not fused to VCCIO so if hw damage is at fault it's not just those pins.
Can you please indicate whether this is expected behaviour or whether there is anything we could or should do to get the board operational?