TUSB321AI: DIR

Part Number: TUSB321AI

Hi team,

Currently using the circuit below, but I found that when the USB-C device is plugged in normally, CC1 = 1.7V, CC2 = 0V, and when flipped (reverse), CC1 = 0V, CC2 = 1.7V. However, my DIR pin is always 0V regardless of whether it's plugged in normally or flipped. The IC is being forced low, and the MUX is not switching at all.

Therefore, when flipped, the USB 3.0 device cannot be recognized. My USB_DET is connected to USB-C power, and the mode is set to DRP mode (haven't tried other modes yet). Could you give me some suggestions on why the DIR pin cannot switch to HIGH?

Schematic: USB_20261114.pdf 

Thanks!

Jeff