Part Number: DS90C031
Other Parts Discussed in Thread: DS90UB928Q
Hi sir,
Except for video transmission, can DS90UB928Q/ DS90UB927Q do i2C touch function on monitor side?
Thanks a lot!
Part Number: DS90C031
Other Parts Discussed in Thread: DS90UB928Q
Hi sir,
Except for video transmission, can DS90UB928Q/ DS90UB927Q do i2C touch function on monitor side?
Thanks a lot!
Hi Sean,
Remote I2C communication:
Yes, the FPD-Link III devices can communicate with remote devices over FPD-Link using I2C.
For example, if you have the host/SoC connected to Ser (eg. 927) and target devices such as MCU or touch connected to Des (eg 928), the I2C transactions can be forwarded from Ser bus to Des bus acting as local proxy controller. This will also use clock stretching.
This app note also explains I2C over FPD-Link: https://www.ti.com/lit/an/snla222/snla222.pdf
Touch controller:
The touch controller can be used if it supports clock stretching and uses I2C. Please also check whether the I2C speed required is within the datasheet specs.
Best regards,
Ikram