TVP5158: TVP5158 Technical Issues

Part Number: TVP5158

Hi ti team,

We are encountering the following issues while using the TVP5158 and need your assistance:

1. Our requirement is to simultaneously input four PAL signals, output via BT.656 to a CPU for decoding, and then transmit the data over Ethernet.
2. I noticed that there is only one digital interface clock signal. Since we have four simultaneous PAL inputs, how many BT.656 outputs are available? How should the clock be connected?
3. If only one BT.656 output is used, can all four simultaneous PAL inputs be decoded at the same time?
4. Could you please provide the hardware design guidelines and reference designs?
5. Based on our requirements, what considerations should be taken into account during the design process?

  • Hello, 

    As indicated on the product folder, there is no design support from TI available for this product so responses are going to be limited to only what can be found in the documentation available in the product folder. 

    Based on review of the datasheet the application should be able to be supported. Section 6 of the datasheet shows an application example where 4 inputs are output on one data lane using interleaving. Interleaving details are in section 3.8.2. Additionally, section 3.8.1 details non interleaved mode where there could be up to four output ports. There is only one clock output, however, so the CPU side would have to be able to take a common clock. 

    Any design support resources are limited to what is available in the product folder. There are PCB layout guidelines here https://www.ti.com/lit/pdf/SLEA073 

    Additionally I did find the TVP5158 EVM user guide, including the schematics, on the web here: https://www.ti.com/lit/ug/sleu108a/sleu108a.pdf. This may be a good resource but I will indicate it should be used as reference only as the EVM is no longer available through TI. 

    Thanks,

    Chris