Part Number: TCAN1044-Q1
Hi team,
"When two TCAN1044 transceivers are connected to the same CAN bus: Transceiver 1 is powered normally and transmitting messages, while Transceiver 2 has VCC at 0V and VIO at approximately 1V. Under these conditions, the CANH recessive level is about 1.1V. However, when the VIO of Transceiver 2 is pulled down to 0V, the CANH recessive level returns to the normal 2.5V. Based on this observation, Transceiver 2 appears to be biasing the CAN bus to GND. Given that the VIO undervoltage threshold is 1.4V, shouldn't Transceiver 2 be in 'Protected Mode' (high impedance) when VIO is at 1V? Should the bus only be biased to GND when the device is in 'Standby Mode'?"
The STB is 0.8V when the CANH recessive level pulls down to 1.1V.
BR
Jiawei