Other Parts Discussed in Thread: TUSB7320, TUSB7340
What I/O standard is prefered for TUSB7320 100MHz PCIe ref clock input?
Is it fine, if provided with 100MHz LVDS clock?
Regards,
Sachin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Elias Villegas,
Can I also use 100MHz HCSL clock for TUSB7320 REFCLK+/-?
Regards,
Sachin
Hello Sachin,
The main difference between the LVDS and HCSL are that HCSL support higher frequencies and more power than LVDS; so if you meet the electrical specs for the TUSB7340 it won't matter what signal type you use.
I don't recommend HCSL due to its high voltage swing which is very close to the maximum input voltage of the TUSB7340.
Regards.