can you please tell me the input capacitance of sn65hvd10 tranceiver IC and the Power dissipation capacitance per latch, F
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can you please tell me the input capacitance of sn65hvd10 tranceiver IC and the Power dissipation capacitance per latch, F
1) The input capacitance as specified in the data sheet is 50pF.
2) We don't specify the powwer dissipation capacitance for full-blown mixed signal transceivers as these do not consist of simple logic latches. The device's maximum current driver capability however is also specified in the data sheet with 60mA.
Regards, Thomas