Other Parts Discussed in Thread: TMDS442
Hi,
we want to use the TMDS442 as a HDMI-Splitter/Switcher.
Is it possible to drive two monitors (Sink ports) from one Source port ?
And I have another question about the sink-priority (SP) bit in the source plug-in status register:
When it is "0" it selects Sink-port 1 as main display.
What happens to Sink-port 2 ?
Is it switched off or does it "clone" the data from Sink-port 1 ?
Thanks in advance,
Ralf Wagner