Other Parts Discussed in Thread: ISO7420FE, ISO7420FCC, ISO7221C
My customer has observed that when input side Vcc is powered UP, and the output side is powered down, when the output Vcc is turned on and rises, The output is high (follows Vcc) until it gets to it's minimum Vin. This signal is used to drive a PWM signal and he would like to have it stay low during power up. Please tell me if a pull down resistor could be used to keep the output low during power up.