Other Parts Discussed in Thread: MAX3232
I am using twoof your parts in a design (MAX3232EI and a SN74LVC16245ADGGR) and I just got errata on the part that interfaces to both of your parts, on power up there will be contention on pins 9 and pin 12 of the MAX3232EI and pins 13,14,16,17,19,20 these pins are outputs and enabled of part # SN74LVC16245ADGGR. Your pins will be driven low with a 33 ohm driver for about 18 ms will this cause any issue for your two parts that I have listed above ? I have no way to fix it but I need to make sure I am damaging your either of your devices. Thank You, Aaron