Other Parts Discussed in Thread: ISO1176T, PROFIBUS
Hi,
The ISO1176T is dedicated Profibus transceiver ISO1176T,
Please check if itcan be used for standard Modbus?
BR,
Rotem.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Profibus requires higher voltage swings (2V vs 1.5V) and less input capacitance (10pF vs 15pF).
Modubus only requires standard RS485 performance.
So YES you can use the ISO1176T for a standard Modbus application.
regards, Thomas