Other Parts Discussed in Thread: DS34RT5110
Hi,
I am having no image issue during the playback using DS34RT5110 evaluation board, I am configuring the DS34RT5110 as such:
BYPASS = low, EN = high, Mode = low, VOD_CRL = 24kohm to GND (DC coupled) .
I used a digital anayzer for the HDMI test (source clock jitter and eye pattern), the test result is really good having at least 50% margin. There is no image when connected to the monitor (SD and LOCK are high!) . I tried to bypass the Reclock and De-emphasis function (BYPASS = high), the image immediately appeared on the monitor. I can't really figure out what is the cause of it?
Can anyone here able to explain on this issue? Thanks.