Other Parts Discussed in Thread: XIO2001
HI,
We are using the following bridge - XIO2001 - PCI to PCIE and have some problems with this bridge:
- Need drivers for LINUX (2.16) On PPC440.
- We need to configure the Bridge as slave device and use an external arbitrator (in this case it's the PPC440).
- The device has no IDSELECT line so initial configuration in this stage is not clear.
- We need help on the configuration process in slave mode, how can we configure the device with no IDSELECT line exists?
BR,
Rotem