Other Parts Discussed in Thread: XIO3130
Dear, Sir.
We are promoting XIO3130 for BD Recorder application.
PCIe is applied as the interface between SOC(Marvell's) and
peripheral Transcoders, etc.
Up-stream port of XIO3130 will be connected to SOC.
I just know that "0" to "31" is assigned as Device # under PC protocol.
I heard that Marvell's SOC assigns "1" as Device #, not "0" for XIO3130.
1. I wonder XIO3130 can work under above situation?
2. Is there a way to solve if there was problem?
Best Regards,
H.Sakai