This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Apparent inconsistency in datasheet for SN65LVDS84

As I dig into the datasheet for the 65LVDS84, I see what appears to be an error.  The Switching Characteristics table on page 5 lists a set of delay times (td0, td1, etc.), which are defined as delays from CLKOUT's rising edge, and refer to Figure 6.  Figure 1 (page 6) is consist with the idea that the new cycle of data output starts after the rising edge of CLKOUT.  However, Figure 6 (on page 9) shows those times referenced to the falling edge of CLKOUT.  Is Figure 6 incorrect?

Thanks,

Scott