This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP or HDMI to 2560x1XXX

Hi,

I've been hunting around for a DP or HDMI to LVDS bridge that supports 2560x1XXX resolution to hook up to an AUO panel.

Does TI have such an offering?

The next best thing I can find so far is the STDP4020 but information on that is quite scarce.

Regards,
David.

  • Hi David, which AUO panel model# do you have in mind?  And how many LVDS channels (or differential pairs for data) does it use?

    Thanks,
    RE

  • Hi, Thanks for the reply. The panel is a 2560x1080 quad lvds so it looks like TI can't help (model no T5706DC01) ParadeTech have the DP628 that looks good too. Shame none of them are as accessible as TI!
  • Another option would be to adopt a 2 chip approach, using a TI based product and perhaps a PixelWorks PA136PD.  Again, we are a smaller company that these larger companies tend to not work or price of entry is massive.

  • Unfortunately, TI doesn't have any quad-channel LVDS serializers.  I think you'd run into issues trying to use two dual-channels in parallel, due to propagation delay differences and the receiver's skew tolerance.  I've seen skew tolerance spec'd in some dual-channel LVDS panels from LG to be up to 1/7th the clock (1 LVDS bit), which is hard to achieve using two separate transmitter devices.

    Best regards,
    RE