This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9509 frequency



Hello,

I can see on the datasheet that it supports 400-kHz Fast I2C Bus operating. And all through the datasheet they only mention that frequency.

Is it a given it works with others too? (I need it to work at 100Khz for my bus).

Best regards.

  • Hi Gabriela,

    That should fine.  The repeater itself is agnostic to the actual bus frequency.  The limiting factor for the bus frequency is determined by the time-of-flight delay through the repeater.  This just means that you can't operate the bus too fast, otherwise, the repeater delays might introduce setup/hold time issues.

    Best Regards,

    Jim