Other Parts Discussed in Thread: XIO2000A
Greetings,
I recently bought a StarTech PCI Express to PCI breakout box which uses the xio2000a chip. My application requires more power than is supplied with the given configuration, they stepdown 12V, 3A, and when I load my PCI cards the power supply is overloaded.
My question is if I were to upgrade the power supply would the xio2000a chip be able to deal with that or is there a power limitation to this package?
I need "<36 Watts" each for 2 of my PCI cards and much less for the last. So maybe 75 Watts total, or about 15Amps.
I'm wondering if I boost the power supply could I damage the xio2000a chip? Currently there is a Silicon Core CX2596
Microelectronics SIMPLE SWITCHER Power Converter Corp. 150 kHz 3A Step-Down Voltage Regulator I would also need to replace.
Any help would be appreciated, since I'm not qualified to design these things!
Thanks,
Jim Lewandowski
Stanofrd University