Other Parts Discussed in Thread: SN65LVPE502, SN65LVPE502A
Hello,
Does TI have recommended settings for the SN65LVPE502 DE, EQ, and OS for the cable-side? Based on the USB 3.0 spec, the best settings appear to be:
OS: NC for 1000mVppd nominal, as per USB 3.0 spec 1Vppd nominal requirement.
DE: NC for -3.5dB de-emphasis, as per USB 3.0 spec -3.5dB de-emphasis nominal requirement.
EQ: ? Since receive equalization training/setting is normally dynamic and cable dependent, what is the recommended single fixed EQ setting to use on the SN65LVPE502 to accommodate USB 3.0 cable lengths of 1m, 2m, and 3m?
Thank you & Regards,
KT