Other Parts Discussed in Thread: DS26LV32AT, DS34LV86T
I'm looking for an IBIS models for the DS34LV86T RS-422 quad receiver. Looking at the data sheet for the TI DS26LV32AT, this part looks to be 100% identical as far as electrical and timing specifications. Even the V-I curves match exactly. Do these two parts share the same design, such that I can use the IBIS model created for the DS26LV32AT to simulate a DS34LV86T? The DS26LV32AT model is available, so hoping this is the case. I would of course use the same package type I anticipate using with the DS34LV86T.
Thanks.