Other Parts Discussed in Thread: DP83848J
Hello folks,
I am planning on using the DP83848JSQ Ethernet Transceiver to add Ethernet to a Xilinx Spartan 6 FPGA.
The DP83848JSQ requests a 25Mhz clock.
I am hoping to be able to cheat and use a PLL internall to the FPGA to synthesize this frequency in order to avoid finding an additional oscillator or crystal, subsequent second sources as well and to save space.
The Xilinx PLL configuration wizard predicts a jitter of about 330pS coming out of the FPGA PLL.
The appnotes and datasheet for the DP83848JSQ do not seem to be consistent with reguards to the max jitter the DP83848JSQ can tolerate.
The datasheet is cool with jitter up to 800pS.
file:///home/user/josh/SmartGaugeStuff/dp83848j.pdf
The appnote on the otherhand would prefer the jitter to stay under 200pS or even 25pS in the short term.
http://www.ti.com/lit/an/snla079c/snla079c.pdf
So what do ya'll recommend? Is the Appnote overspected and the PLL is fine? Or is higher jitter levels known for causing problems and I should really include a seperate oscilator for the DP83848JSQ?
~Joshua