Other Parts Discussed in Thread: DP83848K, DP83848I, DP83620, TLK110
Dear all,
Could you please tell me if there is any way that the auto negotiation can be desabled via an external pin? Maybe the strapp?
How to do that?
Tks and Rgds,
Letice
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Letice,
Auto-negotiation is enabled by default on the DP83848K. Disabling auto-negotiation requires a register write to clear the Auto-Negotiation Enable bit in the Basic Mode Control Register (BMCR), register address 0x00.
Patrick
Letice,
Disabling auto-negotiation using external straps can be accomplished using other devices in our Ethernet portfolio. The following devices provide this functionality and, like the DP83848K, are in the industrial temperature range (-40C to 85C):
Other options are available with additional features (IEEE 1588 hardware support) or additional ports, but the options listed above are the closest to the DP83848K in functionality while still supporting the ability to disable auto-negotiation using external straps.
Patrick