Other Parts Discussed in Thread: AM26LV32E, AM26LV31E, AM26LV31
For the AM26LV32E, do you need to add external termination resistors to the board? Unclear from the datasheet and looking for some guidelines, thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Except for low data rates or very short lines you will require a 100 ohm termination resistor at the receiver input to eliminate reflections on the line.
regards, Thomas
Hi all,
Appending a question to this thread as it seems reasonable to put related subjects together...
I have this project where I link two boards communicating via RS422 (am26lv32e with am26lv31e). It is a uart communication at 921600bps, and cables are cat5e at a maximum of 4 meters.
The termination resistors adopted are 100ohm on each channel of the receivers. This translates into a current consumption of 4x33mA, ~130mA for four channels. Quite high for this project, quite high in a world where we celebrate that a microcontroller can work at 35mA instead of 40mA...
Anyway, does anyone have experience with using higher resistors? Maybe all the way up to 1K or 470r? Would it be stable? Or do you have other suggestions for out next spin of boards, with more efficient components for our case?
Cheers.
Bruno
Folks,
Just got reliable results with 470 ohm termination. Below is a quick print of both A and B channels on the receiver, and for as long as I tested I got zero errors on the incoming counter.
I'm not saying this should be an official solution, just sharing the results so far. Hope this comes useful to others in the future.
Cheers,
Bruno