Other Parts Discussed in Thread: TFP403
Hello,
Can the TFP403 support a 512 x 512 input resolution? According to the DVI 1.0 spec the minimum supported resolution is 640 x 480 @25MHz. If the TFP403 cannot support a 512 x 512 input can it support a 1024 x 1024 input or does the input have to be one of the standard computer or television resolution formats?
Thanks,
Ali