Other Parts Discussed in Thread: TS3USB221A, TUSB2046B
Hi,
I need design like, USB 2:1 De-multiplexer (which has two inputs and one output) output should be connected to 1:4 USB Hub.
I mean, need to switch USB Hub between two USB Hosts based on some enable signal.
I selected ts3usb221a as a De-multiplexer and tusb2046b as a USB Hub. Can I use these two ICs for my requirement.
If not, Could you please suggest me best suitable ICs for my requirement.
And also, please provide me the schematic for this design.
I have a one query, while switching from one host to other, do we need to give reset to USB Hub chip?
What is the purpose of RESET input signal of USB Hub(tusb2046b).
Thanks,
Raju.