Other Parts Discussed in Thread: TUSB1310A
Hi all,
I notice an jitter on PCLK (250MHz).
The TUSB1310A is running with a reference clock of 40MHz and the strapping option-pins for 40MHz are set. All the different power sources are clean. The 40MHz ref-clock and the 60MHz Ulpi-Clock are clean.
Only the 250MHz clock has a frequency jitter. After around 100 clocks (400ns) the clock edges have an jitter of around 2ns.
Has anyone else noticed such jitter? Is this amount of jitter OK?
Is there a special reset sequence required to initialize the chip internal PLL? My current sequnce is to release RESETN first then PHY_RESETN.
Best regards, Elmar