Other Parts Discussed in Thread: TUSB2046B
Hi,
We are running into some trouble attempting to use the TUSB2046B on our USB 1.1 bus. At the moment we have the hub connected to a windows 7 machine for testing. The hub is running in self-powered mode using a 48 Mhz clock. Our design is based on the IT reference schematic as well as the datasheet specifications. Our problem is with the following from the FAQ:
Do we have pull-up on DP0 or DM0, and what is the difference between the two implementations ?
According to the USB specification, you must connect a pull-up resistor of 1.5 kΩ on D+ for a full-speed device or on D– for a low-speed device.
When we connect the 1.5 kΩ resistor to D- for low-speed devices our test units as well as the controller do not recognize the hub. However, if we move the resistor the D+ input the unit becomes functional. Any ideas why this is happening as we are using a low-speed bus ??
(Schematic can be provided to IT employee upon request)
Thank you,