Other Parts Discussed in Thread: MAX202
Hi,
I am using a MAX202IDG4 in the exact same configuration shown in the datasheet. I am using 100nF X7R 50V capacitors.
The application is in an LED light. I have noticed that if the ambient get to over around 50 deg C, then I try to send a command, the command is received correctly however the reply (DOUT2) is not within spec.
It seems to only happen if the unit is hot *before* sending a command. If the unit is cool, then the serial port accessed, there are no problems - even if the unit heats up in the meantime!
It's not isolated to one or two boards, but the whole batch (20+ units).
I've put a scope on the RS232 level RX and TX lines, and when it fails, it shows the TX 'mirroring' the RX line, but very badly deformed and only peak to peak of around 4V. When temp drops below 45degC the TX returns to normal looking signal.
Any thoughts? I've tried putting in 1uF caps and the same thing happens. Its really strange that once it's working, it keeps working - even over 60degC!
Warm Regards,
Sasha.