Hi, I am freshman in electronics design. Recently, I was troubled by the power and signal design in PCB board. I hope someone can help me, thank you.
I have two PCB board, PCB A and PCB B. There is information exchanging these two PCB ,but PCB A and PCB are powered by separated power(5V DC power).
At first, I just connect the signal wires between PCB A and PCB B, then I find both PCB A and PCB B can't work well.
Then I realize that the Ground of these two PCB board should be connected together. After that, these PCB boards begin working, but they get wrong data frequently.
At last, I make these two PCB powered by one power, then they work well.
----
My question:
How the power and signals design between tow PCB board which powered by separated power.
Thank you.