Other Parts Discussed in Thread: TUSB9261
Considering using the TUSB9261 in an embedded design running linux on an arm processor. The datasheet states that "In the absence of an attached SPI flash memory or a valid image in the SPI flash memory, the firmware will idle and wait for a connection from a USB host through its HID interface which is also configured from the bootcode. The latter can be accomplished using a custom application or driver to load the firmware from a file resident on the host system."
Where can we find sample code / drivers to accomplish this. We don't want to use SPI flash memory.