This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1982 - PLL Lock Detection

Guru 19785 points


I understand the "LOCK_CTRL" (Register 01h) programs the maximum phase error between PLL1's Phase Detector inputs.

Is the allowable phase error set by LOCK_CTRL  based on (Hsync input / reference divider) or (VCXO clock / feedback divider) ?

I am thinking the allowable phase error is based on (Hsync input / reference divider).

If the (VCXO clock / feedback divider) timing is inside +/- allowable phase error, PLL1 is locked.

  • Hi Kawai,

    Again, answers to these questions can be found in the following E2E forum post:
    http://e2e.ti.com/support/interface/high_speed_interface/int-high_speed_interface/f/140/p/178827/691492.aspx#691492

    Regards,
    Alan

  • Hi, Alan-san,

    Thanks for your comment, but I could not find the page which you had told me.

    When I jump to the URL, the page shows,

    "Group Not Found
    The requested Group cannot be found."
    Do you need permission to access the page ?
    Best Regards,
    Kawai
  • Hi Kawai-san,

    Sorry, the link I sent was for an internal website.  Here are some answers to your questions:

    Lock Detection for PLL1
    The phase differences between phase detector (PD) inputs produce different up/down output pulses to drive the charge pump and servo the loop filter / VCXO control voltage.  When the PLL is in a "locked" state, the up/down pulses will present equal pulses with minimum width to the charge pump inputs.  For PLL1, the up/down pulse width is compared against the time window (delay circuit) programmed via LOCK_CTRL register.  When the pulse width is within the window for 3 consecutive PD cycles, then valid lock is indicated (SD_LOCK = 1).  When the pulse width is outside the window for 3 consecutive PD cycles, then loss of lock is indicated (SD_LOCK = 0).

    Lock Detection for PLLs 2/3/4
    The phase differences between the PD inputs produce different up/down output pulses to drive the charge pump and servo the internal loop filter/VCO control voltage.  When the PLL is in a "locked" state, the up/down pulses should be equal with minimal width to charge pump inputs.  For PLLs 2/3/4, the time window is based on 2 inverter delays (~50 ps window, default), but this can be programmed to 6 inverter delays (~150 ps window) via a Reserved register 0x1Ch[bit 2].  Valid register values are 0x00h (2 inverter delays) or 0x04h (6 inverter delays).  When the pulse width is within the window for 3 consecutive PD cycles, then valid lock is indicated (SD_LOCK = 1 for PLL4, or HD_LOCK = 1 for PLLs 2/3).  When the pulse width is outside the window for 3 consecutive PD cycles, then loss of lock is indicated (SD_LOCK = 0 for PLL4, or HD_LOCK = 0 for PLLs 2/3).

    Regards,
    Alan

  • Alan-san,

    Thank you for the answer.

    Best Regards,

    Kawai