Other Parts Discussed in Thread: LMP91000
Hello, I intend to use LMP91000 with a standard electrochemical cell with three electrodes with graphite working electrode, they may be used in most of analytical applications. Every serygraphed sensor is made by a 3 mm diameter circular graphite electrode and a pseudo-reference silver electrode and a graphite counter-electrode electrode.
I wonder how to obtain the electrical features to create a "New" Sensor in Webench.
Sensitivity (na/ppm) = 1 ; It's an amperometric application, I need to measure currents in the range 0 nA - 1000 nA
Full Range Scale (ppm) = 1000
Zero level (nA) = ?
Bias Voltage = 200 mV
Rload = ?
Capacitance = ?
Resistance = ?
The manufacturer EcoBioservices (http://www.ebsr.it/GSensor_eng.html), seems not to have these values...
Thank you !!!
Alejandro