Hi
My requirement is to test the PHY DP83848 in RMII mode and MII mode with the same circuitry. I have used 25Mhz clock oscillator for MII modeand 50Mhz Osc for RMII mode , which are selected using MUX with a control pin. My question is , whether the RXD{0..3} and TXD{0..3} can connected in both the modes? usually in RMII mode only RXD0,1 are used and RXD2,3 should be open similary TXD0,1 are used and TXD2,3 are GNDed. Can we use a mux logic to connected to the PHY in MII mode and Open/GND in RMII mode ? ( RXD,TXD - 2,3 signals).
regards
Jonna