Other Parts Discussed in Thread: TUSB6250
Hi,
I need to interface a cmos based camera to a USB 2.0 host module.
Currently, the camera gives 8 bit parallel data output. There are also control lines (VSYNC, HSYNC, PCLK) and I2C configuration lines available on the camera module.
The camera gives a resolution of 640x480, and frame rate of 25 frames per second. Hence the total data comes to about 7.3MBytes per second.
The USB 2.0 HS supports upto 480Mbps, which I think should be enough for taking the data from the sensor.
Can you please suggest me a controller which I can use for this interface ? Can I use TUSB6250 for this purpose ?
Thank You
With Regards
GIGIN JOSE