This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25CP102 / Internal failsafe bias circuit

Other Parts Discussed in Thread: DS25CP102

Hi,

The datasheet of DS25CP102 does not state about internal failsafe bias circuit, but I understand that these devices has it although it is not stated in datasheet.

How can we inform customer about internal bias voltage for devices which does not state the spec definitely like this DS25CP102.

Best Regardes,


  • Greetings -

    I also reviewed the datasheet, the device does provide an EQ input and also interanl 100 Ohm termination resitsor, but I do not seen any mention of a failsafe state or suport.  I do not believe that is included based upon the datasheet. If failsafe is needed, external pull up and down should be used and set a bias greater than the threshold.

    John Goldie

  • Goldie-san,

    Thank you for your response.

    I will inform customer that they should need to add external failsafe bias for safety if they need.

    Best Regards,

    Sonoki