Other Parts Discussed in Thread: SN65C1168, SN751177
I need to have an RS-485 Transceiver Component solution equivalent to the 75ALS1177NSR but can handle the operating temperature range from -40C to +85C. The SN65C1167ENS can handle the temperature requirement but it is not RS-485 compliant. Which other TI Component should I look into?
The TI SN65C1167ENS is not compliant to RS-485 and we saw it cannot handle driving more than 5 device loads in our products. However, if we replace it with the TI 75ALS1177 Driver, it can drive 6 device loads ok but this part can only operate from 0C to 70C. Please help to search a dual Transceiver Device that is industrial temperature rating from -40C to 85C and complies to RS-485.