This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83865 Interop Issues with switches

Hi,

There is an issue with the DP83865 with a customer using in conjunction with a switch.

Two particular models of switches yields corrupted data link.

The block diagram is simple.

Xilinx FPGA <-> DP83865 <-> Switch

The gig switch includes the following: dlink dgs 3200-10  and cisco catalyst 3560g-24ts-s.

If the customer inserts a "working" switch between the "failing" switch, the system links correctly and data is transferred without corruption.

Please provide some suggestions. Customer has reviewed the  documented located at   http://www.ti.com/litv/pdf/snla065

The customer has followed the suggestion with no resolutions. Please advise.

Wallace