Other Parts Discussed in Thread: TUSB9260
Hi,
We are developing a USB 3.0 to SATA II converter. In that we are plan to use TUSB9260 controller. Now i have following queries, Please Clarify immediately.
A) Data Manual of TUSB9260 speaks about configuration of controller from external flash memories and firmware resides on the flash device. Now should we develop the firmware or TI provides us the firmware. If so how do we load the firmware.
B) One of my requirement states that the device should be detected by the windows file manager. This means the TUSB9260 controller with 512k bytes should be detected by windows as a separate disk drive. When I connect the SSD to the controller, there should be two disk drives or how?: Like One the TUS9260 controller with flash memory and second one with SSD drive. Please clarify.
C) Does the controller support, SATA SSD HOT plug-unplug.
D) What can be the maximum size of the flash memory we can use ?. If i want to write my Company name to it, that is when the device is detected, our company name should pop as like any external devices or how?
E) Is there any product already available in the Market with using TUSB9260? If yes, please give me the product details and share the product photos.
Looking for TI experts reply quickly.
Thanks,
Ganes.