Other Parts Discussed in Thread: MAX3221-EP
I am trying to complete a power consumption estimate for a design and the datasheet for the MAX3221-EP has me confused.
At the bottom of page 3 in the datasheet the supply current is given for a number of different scenarios. I don't plan to use the auto-powerdown feature so the top most supply current rating is the most applicable to my situation. This value is listed as 2mA max, however, one of the criteria is "no load." This chip will be driving another device which I do not have detailed design information for other than that the interface is EIA-232 compliant.
My questions are:
- Is this max current rating still a reasonable estimate for when this chip is loaded down with another EIA-232 device over a short cable?
- Does the provided current value assume the maximum possible datarate (250kbps)?