Other Parts Discussed in Thread: TLK110, AM3359, DP83849IF, TLK106
I am looking at the AM3359 for an Ethercat application. The Industrial Communications eval board uses two TLK110's on it. The TLK110PT offers "RT" ( RealTime ) Deterministic, Low Latency, Low Jitter ) performance.
It looks like the DP83849IF offers the same "RT" features, however when I look at the datasheets for the two devices, I see slightly different wording that makes me wonder if the DP83849 is suited for EtherCat Industrial COmmunications. My assumption, also, is that the DP83849 was not a released product when the AM3359 board was designed?? -or- perhaps, it's just not a good choice to design in.
Does the DP83849 offer the same performance as two TLK110's? Is there a reason NOT to use a DUAL PHY in an EtherCat application? This could be a nice space saving way to go.
Thank you,
Bryan Busacco.