Other Parts Discussed in Thread: TUSB8040A
Hello,
I've designed a USB HUB using TUSB2077. It works fine, but just at USB 1.1. When I plug it into the PC, the typical message pops-up "This device can perfom faster".
We are using a 6 MHz XTAL with MODE pin tied low.
Here is the sch, with no pull-ups on OC# pins, but they actually are in the PCB (that's why it works, at least at 1.1)
I followed all the specifications... Low ESR 100uF caps. XTAL circuit cap.s ans res. I don't know, I guess it's just a matter of a little detail, but I can't see it.
Thank you.