Other Parts Discussed in Thread: 4460, SN65LVDS315, SN65LVDS31
Hello,
We are interfacing OMAP 4 to two CMOS camera module. First is connected to the parallel interface, but the second one does not directly connect to the CS interface.
The camera parallel interface output has 10-bits. Can we use two 8-bit TI converters, one for each lane, where the first one is conencted to bits 0-7 and the second one to bits 8 and 9, or is there a converter for 10-bits?
Thanks for the help.
Regards,
Tim