Other Parts Discussed in Thread: LMH0307, LMH0394, LMH0344, LMH0384
Team,
My customer has the following question:
Regarding termination of the LMH0307, the datasheet discusses 75 ohm output pull-ups with a 750 ohm RREF resistor. I installed 50 ohm pull-ups to provide a 100 ohm differential output. It looks like the RREF resistor needs to change to 500 ohms as well otherwise I don't get the specified output voltage levels. The datasheet is adamant it should be 750 ohms, however it only addresses 75 ohm terminations. Am I correct the RREF resistor needs to be 10 times the single ended termination resistor value to generate the correct output voltage level?
Regards,
Aaron