Other Parts Discussed in Thread: DS90C387A, TFP403
Hi,
I am currently working on a DVI LVDS bridge. I will use the TFP403 in combination of DS90C387A. So after 2 weeks and lots of applications notes I have made a schematic (schematic attached 6153.DVI _LVDS.pdf) for it
I will use this board with an LG Panel (datasheet attached 6712.ASUS_ML229H_LM215WF3-SLC1_Datasheet.pdf), so I have some question...perhaps somebody can help me.
1. LVDS output of the DS90C387A are A0 - A7 but I have to know If the first 4 are even or odd (see page 10 of LCD datasheet).
2. User control pins CLT1/CLT2 has to be connected or can I leave them NC?
3. Are my connection for RSVD correct? (Pin 42)
4. Which type of elkos to you suggest?
5. I use ferrit beads which have 600ohm@100MHz is that ok?
For starting PCB I have read some guide lines from you. Is it really necessary to have an 4 layer design? If yes will this layer configuration work: signal/VCC/GND/signal?
I know I have a lots of question but I hope somebody can help me!
Best regards,
Juergen