Other Parts Discussed in Thread: TUSB1310
Problem:
While working with BSDL file of TUSB1310 I have encountered the following warnings: ( Perhaps it is not the latest BSDL file?)
1) All paragraph references are to IEEE Std 1149.1-2001 Para: B.8.13.3.b Line 309 in document TUSB1310_sp1_rev0_2.bsdl at circuit location X Expecting: REGISTER_ACCESS for instruction PRELOAD not found
2)
Para: B.8.14.1.3
Line 388 in document TUSB1310_sp1_rev0.2.bsdl at circuit location X
Message: FATAL ERROR. Incompatible pin/cell types. INPUT cell 51 and BIDIR cell connected to 'inout' port, PHY_STATUS
/////////////////////////
Para: B.8.14.1.3
Line 391 in document TUSB1310_sp1_rev0.2.bsdl at circuit location X
Message: FATAL ERROR. Incompatible pin/cell types. INPUT cell 54 and BIDIR cell connected to 'inout' port, RX_ELECIDLE
/////////////////////////
Multiple instances of CELL Function definition problems,Para. B.8.14.1.3
/////////////////////////
Warning Summary: 4 warnings.
These warnings may not prevent test generation, but should be checked.