Other Parts Discussed in Thread: LMH1982, LMH1982APP-SW
LMH1982 Application
If the input format is 625i and the output format 1080i/50 ,then how to program the register and what is the programming sequence?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMH1982, LMH1982APP-SW
LMH1982 Application
If the input format is 625i and the output format 1080i/50 ,then how to program the register and what is the programming sequence?
Hi Gang,
Programmming of input format and output format are covered in section 4 and 5 of the LMH1982 datasheet. Also refer to Table 1.
You can also download the Eval software GUI which shows register programming for different input and output formats.
http://www.ti.com/tool/lmh1982app-sw
Regards,
Alan
Hi Alan,
I understand from the data sheet that there is a suggested sequence that the registers should be programmed.
Is there a way of showing the sequence and register values that are generated when using the LMH1982 Application v2.0 program without using the USB interface, as I do not have an evaluation board.
This sequence information would make it far easier to program the LMH1982 using the I2C interface of the microcontroller.
regards
John